AnsweredAssumed Answered

AD9653--EVALUATION BOARDS

Question asked by xing_qianjin on Dec 6, 2017
Latest reply on Dec 9, 2017 by xing_qianjin

Hi,

In my project, I use AD9653 as the High-speed ADC with a sampling clock at 80MHz.The reference voltage of ADC is 1V.The frequency of the analog signal(sin and cos ) are 40kHz,and the amplitude of the analog signals is 2Vpp(after difference).But the data I got have noise,so could you sent me the data  collected by AD9653 EVALUATION BOARDS,the test conditions are in accordance with my project as much as possible . Then I can analyse the data and improve my PCB board.

My email is 875994877@qq.com.

Thank you !

Outcomes