AnsweredAssumed Answered

Faster CF Card Performance in True IDE Mode

Question asked by sirspot on Nov 11, 2011
Latest reply on Nov 13, 2011 by sonic

I would like to increase the read  throughput of the CF card on my custom uClinux based BF537 board.  We  have the CF card configured for True IDE Mode.  It works well but slower  than expected.  Here are the results of a read test:

 

root:/> hdparm -t /dev/sda1

/dev/sda1:
Timing buffered disk reads:    3 MB in 3.13 seconds = 981 kB/s

 

We  should be able to get much more than 1MB/second.  It seems like the  card is operating in PIO0 mode but should be able to operate in PIO4.   Here is what happens when I load the driver using this command:

 

modprobe pata_platform.ko

 

scsi0 : pata_platform
ata1: PATA max PIO0 no IRQ, using PIO polling mmio cmd 0x20300020 ctl 0x2030001c
ata1.00: CFA: SanDisk SDCFX-4096, HDX 3.20, max MWDMA2
ata1.00: 8027712 sectors, multi 0: LBA
ata1.00: configured for PIO
scsi 0:0:0:0: Direct-Access     ATA      SanDisk SDCFX-40 HDX  PQ: 0 ANSI: 5
sd 0:0:0:0: [sda] 8027712 512-byte logical blocks: (4.11 GB/3.82 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI removable disk

 

When  I set the pata_platform module parameter pio_mask=31 then the above  reads: "PATA max PIO4" but the transfer speed does not improve.  After  looking through the pata_plaform driver a bit it doesn't look like it  ever tries to send the ATA command to set the PIO mode.

 

Please  provide instructions on how to increase the read performance of the CF  card in True IDE Mode.  We are currently at 8Mbps but I would like to  get as close to 13Mbps as possible.

 

Thank you,

Adam

Outcomes