AnsweredAssumed Answered

Force ADP5062 to do power off cycle

Question asked by Veletsu on Nov 20, 2017
Latest reply on Nov 22, 2017 by Veletsu

Is it possible to do hard power off cycle with ADP5062 charger. We do have a need to be able to do a complete power off reset to the board and restore the situation without need to plug in the external charger.

 

We have a lithium battery powered device with 5V voltage from external charger to VINX pins.

 

We do have Pull up resistors (powered from a regulator in ISO_SX) in DIG_IO1 and DIG_IO3 pins and DIG_IO2 is floating. Thus: charging is enabled and chip is active whenever the device is powered.

Outcomes