AnsweredAssumed Answered

Compile error ADAU1452 Master control port SPI

Question asked by wygonski on Nov 20, 2017
Latest reply on Dec 20, 2017 by DaveThib

I'm trying to use the Master Control Port IO block in SigmaStudio v3.15 build 3.   The release info for 3.15.2 beta says it's supported:

"Master Control Port Runtime Sequential Write and Master Control Port Boot time I/O now supports SPI protocol along with I2C."

 

My simple schematic contains only one Master Control Port IO block configured for SPI:

SigmaStudio compile error

However, I get a compiler error when downloading to EVAL-ADAU1452:

###### IC 1 ######
ADAU145X Assembler, Analog Devices Inc.
Version: 3.15.3,1737 (built 9/29/2017)

##### Compile Started: Sunday, November 19, 2017 10:26:27 PM #####
error (44,ControlPort12): The name 'i2c_speed0' in memory 'DM0' is undefined in module __MASTER_CONTROL_PORT0__ (732)
error (45,ControlPort12): The name 'i2c_address_bytes0' in memory 'DM0' is undefined in module __MASTER_CONTROL_PORT0__ (733)
##### Compile FAILED: 2 errors, 0 warnings #####

 

Is this feature supported in 3.15 build 3?   If so, why the compile error having to do with I2C?

Outcomes