AnsweredAssumed Answered

Using AD595 for K type thermocouple and 10 bit ADC of 8 bit microcontroller how to measure full range temperature  i.e. up to 1350 deg Celcius

Question asked by d67uttam on Nov 19, 2017
Latest reply on Nov 21, 2017 by ARoxas

I want to do an experiment with K type thermocouple and AD595  and to display the temperature in a LCD display. I want to use 8 bit microcontrolller with 10 bit A to D converter,  

AD595 shows 10mV/deg C so max  (5000mV/10= 500 degC can be achieved/displayed, but K type thermocouple range is  max 1350 degC, 

now my question how to show this max temperature  by using AD595 and 10 bit microcontroller (5.5 volt is its max operation voltage)

Outcomes