AnsweredAssumed Answered

ADF5356, read LOS(loss of signal)

Question asked by Erlend on Nov 16, 2017

On ADF5356, is it possible to read the loss of signal-indicator some way?

 

I want to do a start-up with PFD>76 MHz and the setup require a two-step programming.

 

I just want to be sure the reference is in place first, otherwise I don't expect it to recover later.

 

The application note for fast locking hints of extra functionality (mostly "Reserved")

Outcomes