AnsweredAssumed Answered

AD9250-250EBZ on HSC-ADC-EVALEZ

Question asked by LuDi on Nov 14, 2017
Latest reply on Jan 5, 2018 by LuDi

Hi

I got a AD9250-250EBZ Evaluation Boards, it is a old version board and didn't have a FMC connector, so I bought a CVT-ADC-FMC-INTPZB board.

Can I use these two board on a HSC-ADC-EVALEZ? I read your EVAL-AD9250 page, I thought a old version AD9250-250EBZ with a CVT-ADC-FMC-INTPZB could work on HSC-ADC-EVALEZ just like a AD9250-FMC-250EBZ dose. But when I connect them all together the SPI controller could not recognize the evaluation board(the Visual Analog could recognize the HSC-ADC-EVALEZ, and the program was succeed with a DONE led lighting up).

Is there any configurations need to be changed on AD9250-250EBZ/HSC-ADC-EVALEZ? Or is the old version AD9250-250EBZ could only use on HSC-ADC-EVALDZ while the HSC-ADC-EVALEZ could only work with AD9250-FMC-EBZ?

 

Best Regards

Outcomes