AnsweredAssumed Answered

AD916x-FMCx-EBZ & ACE

Question asked by Mochi on Nov 12, 2017
Latest reply on Dec 8, 2017 by Mochi

Hello
Please advise about AD9163-FMCC-EBZ.
My customers are experimenting with this evaluation board by combining the Xilinx Artix-7 FPGA AC701 evaluation kit.
The experiment is not going well.
They are trying to connect using JESD 204B, but the handshake is not established.

They did not verify the signal from the USB cable, but on the evaluation board
Since the LEDs of "ADF 4355 Locked" and "Interruption" are lit, it seems that the control of "AD 9163" is done.

Also, since the output as intended is output to OUT 0 (GBTCLK 0_M2C_P/N) of "AD 9508", it seems that the control of "AD 9508" itself is also possible.
However, in that state there is no output in OUT 2 (SYSREF 2_P/N) and OUT 3 (SYSREF_P/N), and even if "Read All" is executed, all the registers will be "0" in return value.

Why can not they do?
I would be pleased if you could give me advice.

Best regards

Outcomes