AnsweredAssumed Answered

AD2S1210 LOT indicate

Question asked by sss on Nov 9, 2017
Latest reply on Feb 9, 2018 by jcolao

Hi all,

 

In the datasheet 17 page at AD2s1210, 

Loss of Position Tracking Detection

LOT can be indicated for step changes in position (such as after a RESET signal is applied to the AD2S1210).
It is also useful as a built-in test to indicate that the tracking converter is functioning properly.

 

What does it means,  "for step changes in position" ?

As in the following, if the resolver indicates the LOT every step rotation, with every no latch ?

 

           0°→30°→-30°→0°→60°→... continue

LOT indicate↑  ↑     ↑        ↑     

 

Best regards,

sss

Outcomes