AnsweredAssumed Answered

Can  EVAL-HMC7044 generate 2 frequencies on its outputs?

Question asked by AAmiri on Nov 8, 2017
Latest reply on Mar 14, 2018 by AAmiri

Hi, 

I was wondering if the HMC7044 Eval board can be programmed to generate 2 LO/Clock frequencies at the same time on its outputs. One at 3.2 GHz to drive the AD9914 ADC and one at 2050 MHz to drive a mixer. If this is not possible, any alternative options?

 

Edit: I can see there is 1 VCXO output. Is this available on the Eval board? I can presumably use this to connect to another PLL/synth to generate the 2050 MHz frequency? 

 

 

Regards,

Amin

Outcomes