AnsweredAssumed Answered

HMC6300 in FMCW radar

Question asked by limimat on Nov 8, 2017
Latest reply on Nov 29, 2017 by Mark_D

Is HMC6300/HMC6301 suitable for FMCW radar application? We have external source which can generate frequency sweep for example 200MHz to 900MHz. I would like to know that could HMC6300 be used to upconvert it to 60GHz and HMC6301 to downcorvert back to "baseband" so that phase change that happen in channel at 60GHz is preserved. We would do the phase detection at baseband signal in external device. And should both I and Q baseband inputs be available for HMC6300?

 

Regards Matti

Outcomes