AnsweredAssumed Answered

For the AD5721R what mode should I select if I use VDD=+5.5V and VSS=-5.5V to generate a  +/-4.5V Vout? Shall I use m=8 and c=4 ( +/-10V range) or m=4 and c=2 ( +/-5V range) ?

Question asked by jop_ny on Nov 7, 2017
Latest reply on Nov 9, 2017 by jop_ny

The transfer function is:

 

#AD5721R range setup

Vout can not reach +/- 10V if VDD=+5.5V and VSS=-5.5V. Vout can only reach +/-4.5V due to the 1V drop. But how shall I program RA to get +/-4.5V Vout?

 

 

The documentation states that the register RA is used:

Outcomes