AnsweredAssumed Answered

Unstable JTAG connection to target board

Question asked by col on Nov 8, 2011
Latest reply on Nov 10, 2011 by hackfin

Hi

 

I have the analog devices ADZS-USB-ICE and trying to connect it to the ADSP BF504 on my DSP board.  May be 1 out of 10 times I can establish a connection but most of the time I can't.  Every time it failed to establish a connection I ran ICE test and all the tests passed (i.e.

Openning Emulator Interface -Pass

Resetting ICEPAC module -Pass

Testing ICEPAC memory -Pass

Determinging scan path length - (detects 1 device)

Performing scan test -Continous scan up to 10 Mbytes (Pass)

 

Even after ICE test passed, I still can not establish a sesstion in VDSP++.  I have checked all the power supply/ground pins, input clock to DSP, reset pin of DSP, PG pin (pull low), and Wake_up pin (high) and they all checked out.  Here are what I have checked:

 

ADSP BF504 (88pins):

VDDC (core voltate) = 1.2V

VDDIO (I/O voltage) = 2.5V

Reset Pin = Pull up high (10K to 2.5V)

PGn = Ground

clock in (pin 68): 12MHz

XTAL pin = no connection

 

 

Visual DSP/Emulator Setup:

Visual DSP++5.0 Update 10 (Product Version 5.0.10.0, IDDE version 8.0.7.15, Build Date: July 5, 2011)

Visual DSP++5.0 License:  Blackfin Demo-Full (Expiring in 37 days)

Visual DSP++5.0 Configuration (Type: USB-ICE, Emulator Settings Device ID: 0, Emulator Settings JTAG I/O Voltage: 2.5, Device 0 Type: ADSP-BF504, initial connection option:  Halt and reset.)

 

Deleted and installed the driver for the ADSP BF504 and still no help.  Deleted and re-create session and still no help.

 

Like I said, ICE test always passed but then unable to establish a conection (most of the time) to target board in Visual DSP++5.0 (always getting error code 0x80044005)

 

Thanks,

 

Loc

Outcomes