AnsweredAssumed Answered

Wireless video

Question asked by VeyDlin on Oct 31, 2017
Latest reply on Nov 5, 2017 by VeyDlin

Hello

 

I want to make video monitor HD720 30Hz, the transmitter board should not be greater than 150x15mm which is why I can't use the big processors.
Also I can't afford to use BGA in increments less than 0.8 mm because it is a very increased cost of device.
I want to put a LVDS/rgb666 display on the reception.

 

What can I use to accomplish this?
I wouldn't want to use Linux because it really increases the design time for me.
It will be very good to have as many code as possible for the example .

 

Thank

Outcomes