AnsweredAssumed Answered

ADXL356 and temperature sensor

Question asked by Mochi on Oct 30, 2017
Latest reply on Oct 31, 2017 by Mochi
I have a question about the temperature sensor built into ADXL356.

I read the datasheet.(Data Sheet ADXL356/ADXL357 Rev. 0)
In the datasheet, it is stated that the temperature sensor has a slope of 3 [mV / ° C] and an intercept of 892.2 [mV] at 25 ° C.

However, in the chart of the same data sheet, it is stated that the temperature sensor has a slope of 3 [mV / ° C] and a intercept of 980 [mV] at 25 ° C.


I am aware that the value of 892.2 [mV] is a TYP value.
Is it OK to interpret both tables and charts as correct?

Best regards

Outcomes