AnsweredAssumed Answered

AD7193 Driver with Raspberry Pi

Question asked by SKR on Oct 30, 2017
Latest reply on Jun 28, 2018 by neeraj1998

Hi,

So i have been trying to to establish SPI communication between AD7193 and Raspberry pi 3. I'm using the Yocto-rpi image for this purpose. This is procedure i followed but facing some issues:-

1. Enabled the ad7193 driver in menuconfig.

2. Added the patch file in the drivers/staging/iio/adc/ad7192.c for it to support device tree.

3.Created an overlay. dts file for this is /boot/dts/ as follows

/dts-v1/;
/plugin/;

 

/ {
        compatible = "brcm,bcm2835", "brcm,bcm2708", "brcm,bcm2709";

 

        fragment@0 {
                target = <&spi0>;
                __overlay__ {
                        status = "okay";
                };
        };

 

        fragment@1 {
                target = <&spidev0>;
                __overlay__ {
                        status = "disabled";
                };
        };

 

        fragment@2 {
                target = <&spidev1>;
                __overlay__ {
                        status = "disabled";
                };
        };

 

        fragment@3 {
                target = <&gpio>;
                __overlay__ {
                        ad7193_pins: ad7193_pins {
                                brcm,pins = <45>;
                                brcm,function = <0>;
                                brcm,pull = <0>;
                        };
                };
        };

 

        fragment@4 {
                target = <&spi0>;
                __overlay__ {
                        /* needed to avoid dtc warning */
                        #address-cells = <1>;
                        #size-cells = <0>;

 

                        adc: ad7192@0{
                                compatible = "adi,ad7192";
                                reg = <0>;
                                pinctrl-names = "default";
                                pinctrl-0 = <&ad7193_pins>;

 

                                spi-max-frequency = <1000000>;
                                spi-cpha;
                                spi-cpol;
                                irq-gpio = <&gpio 45 0x2>; /* IRQF_TRIGGER_FALLING */
                                interrupts = <45 0>; /* high-to-low edge triggered */
                                interrupt-parent = <&gpio>;
                                adi,reference-voltage-mv = <3300>;
                                adi,clock-source-select = <2>;
                                adi,refin2-enable;
                                adi,unipolar-enable;
                                status = "okay";
                        };
                };
        };
};

 

4. Added this overlay.dts file to bb.append file and rebuild the kernel and enable the overlay file in /boot/config.txt in the target.

5. The driver is loaded but i keep getting setup failed and spi0.0 supply vcc not found, using dummy regulator
ad7192 spi0.0: setup failed

ad7192: probe of spi0.0 failed with error -5

I'm attaching the image below please let me know what i'm doing wrong.

 

Note:- I have connected AGND,CS,SCLK,Din,Dout/Rdy to the respective pins in raspberry pi 3.

Thanks in advance.

-SK

Outcomes