AnsweredAssumed Answered

linux-2016_R1 build fails with AD9680

Question asked by htorke on Oct 27, 2017
Latest reply on Nov 7, 2017 by DragosB

I have an FMCDAQ2 evaluation card running off a demo SD card. This much works fine. I attempted to pull the git repository and rebuild the kernel image as explained here:

 

https://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/software/linux/zynq

 

and an image was successfully built. When I use this image, the following devices are available:

 

ad7291

xadc

ad9523-1

axi-ad9144-hpc

 

Note that the FMCDAQ2's AD9680 does not show up. This is confirmed in the IIOscope application, which shows now devices available.

 

Is there an issue with the current build? I also attempted the zynq-xcomm branch of the git repository, which gave similar results.

Outcomes