AnsweredAssumed Answered

AD9363 setting

Question asked by ramon.righini on Oct 27, 2017
Latest reply on Nov 17, 2017 by ramon.righini
Branched to a new discussion

Hello,

 

I'm using Analog Linux driver for AD9363 in a custom board without the TX.

 

The kernel module prints this warning

" Calibration TIMEOUT (0x287, 0x2)"

it should be related to TX calibration. Can I disable the TX calibration in the DTS file?

 

Further, the device is locked in "alert" state, I need the FDD state for my tests (FDD is specified in DTS).

 

The content of the "state registers" is

0x13   0x1

0x14   0x29

0x15   0x4

0x16   0x0

0x17   0x15

 

I tried to change the register values, but I can't set the FDD state.

 

Do you have any suggestion?

 

Thanks and Regards,

Ramon

Outcomes