AnsweredAssumed Answered

HSC-ADC-EVALEZ+AD9656 Matlab control

Question asked by EDDDD on Oct 19, 2017
Latest reply on Oct 19, 2017 by DougI

Good afternoon.

   I'm working with a set HSC-ADC-EVALEZ +AD9656 in a matlab environment. For work I use the code based on the example provided on this forum. But in the code there are teams whose assignments are unknown for me. For example: board.FpgaSpiWrite (uint16 (hex2dec ('103')), uint16 (hex2dec ('02 ')));

board.FpgaSpiWrite (uint16 (hex2dec ('104'))), uint16 (hex2dec ('00 ')));
board.FpgaSpiWrite (uint16 (hex2dec ('106')), uint16 (hex2dec ('20 '))); 
   Attempts to find some sort of description for these (and other) memory registers were unsuccessful. In the datasheet to AD9656 they are not mentioned. There is someone that have seen a description of these (and other) registers? And there is any detailed description of the API?

Outcomes