Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Sensors
Sensors
Documents What Is the DS1925 Calibration Process?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • +AD5940: FAQ
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • +DS1922L-F5#: FAQ
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • -DS1925L-F5#: FAQ
    • How can the DS1925's memory work when the battery is depleted?
    • Is the DS1925 Mission Start Delay (MSD) different than the DS1922L's or the DS1923's MSD?
    • My DS1925 with a high number of total samples works fine but it can't perform a SUTA mission. Why?
    • Reading the raw contents of a DS1925's "Data Log" memory bank with the OneWireViewer takes over a minute. Why?
    • The OneWireViewer's DS1925 "A to D" tab displays errors. Why?
    • What are the oscillator specifications of the DS1925L?
    • What battery type does the DS1925 Data Logger contain?
    • What Is the DS1925 Calibration Process?
    • What should the OneWireViewer be reading on the DS1925's "A to D" tab on a data logger that is "fresh-from-the-factory"?
    • Why am I getting an incor date in the exported data to a CSV file of a DS1925?
    • Why can't I start a mission on the DS1925?
    • Why is the DS1925's Minimum Recommended Sample Rate 5 Minutes?
    • Will the DS1925 operate outside its specified temperature range?
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • +MAX30001CTI+T: FAQ
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • +MAX30003CTI+T: FAQ
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • +MAX35103EVKIT#: FAQ
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

What Is the DS1925 Calibration Process?

Introduction

This document discusses the calibration details the DS1925’s temperature sensor which provides an accuracy of +/-0.5C over the operating range of -40C to 85C. The DS1925 temperature sensing solution operates from an advanced principle within the electrical engineering field known as “band-gap temperature sensor design1“ whereby Maxim-factory temperature calibration is performed with a process involving the application of a precision voltage during manufacturing.  This differs from previous calibration methods involving the use of temperature chambers in which products are placed and exposed to multiple test temperatures then adjusted for accuracy.  Based on applying external precision voltages to the IC containing the temperature sensor circuit, responses are measured by test equipment to determine the required calibration adjustment to achieve the specified accuracy performance.  Both simulation results and post-calibrated data from temperature chamber studies confirm this methodology.

Temp Sensor Circuit Implementation Details

Fundamentally, the DS1925 uses p-n junctions of a bipolar transistors (BJT) to measure temperature. These BJT p-n junctions are electrically equivalent to a circuit element known as a diode. The electrical characteristics of the BJT diodes have predictable voltage-temperature dependencies that are described with mathematical equations enabling them to be used as temperature sensors. The DS1925 uses two BJT diodes, with voltages Vbe1   and Vbe2  , as shown in Figure 1.


Figure 1: Transistors Configured as Diodes

A constant current through each diode in Figure 1 produces the temperature dependence of the base-emitter voltage (Vbe  ) described by Equation 1. Since the bias current sources are different, the results are two distinct base-emitter voltages. The ∆Vbe   is the difference of the base-emitter voltage measurements from the two excitation currents.
 
∆Vbe= K*Tq* ln⁡(Ic1Ic2) Eq. (1)
Where:
∆Vbe=Vbe1-Vbe2  Eq. (2)

Equation 1 is for an ideal transistor, so a non-ideality factor (η  ) is needed for real world usage.  Applying this adjustment, Equation 3 is the fundamental BJT base-emitter diode voltage equation.
 
∆Vbe= K*T*ηq* ln⁡(m) Eq. (3)



Where:
m= Ic1Ic2    (constant and known by design)
K   = Boltzmann's constant
T   = circuit operating temperature in Kelvin
q   = constant charge on an electron

With Equation 3, from a known ∆Vbe   the temperature T   of the DS1925 sensor, and therefore the DS1925 operating condition, can be precisely determined.

Advanced Single-Point Calibration

Unlike traditional calibration techniques requiring multiple temperature points and precise references, this advanced single-point calibration methodology does not require either one. This section presents the principles and methodology used to calibrate the DS1925’s temperature sensor, which does not require a forced IC temperature or a reference temperature sensor to measure the actual IC temperature. Instead, it relies on applying a high-precision external voltage to the device under test (DUT) to determine its temperature followed by adjusting, and therefore calibrating, it’s Vbe   to an ideal characteristic2. Once performed at temperature T  , this calibration allows Vbe   to be precisely known across all operating temperatures. There are two steps to the calibration process:
  1. Through application of a precision voltage by test equipment, determine the actual temperature (T  ) of the DS1925 IC.
  2. Adjust and calibrate Vbe   such that it’s value at T   is equal to ideal.
 
 
Calibration Step 1
Figure 2 shows the DS1925’s internal analog-to-digital converter (ADC) and the various inputs. Equation 3 has two unknowns: temperature and ∆Vbe  . We can configure the DS1925 ADC to select Vbe  1 & 2 as its references and apply a precision external voltage (Vext  ).


Figure 2: DS1925’s Internal ADC and Inputs



The resultant ADC code from applying an external voltage Vext   is:
 
ADC Code= ∆VbeVext+∆Vbe Eq. (4)

Since the ADC code was read from the device and the externally applied voltage Vext 
is known, we can solve for ∆Vbe   in Equation 4.

Next, with ∆Vbe   known, solving for temperature in Equation 3 gives:
 
T= ∆Vbe*qK*η* ln⁡(m) Eq. (5)

This temperature value T   determined from Equation 5 is the precise operating temperature of the DS1925 at this test step and used for the next step in the calibration process.

Calibration Step 2
With T   known, a precision ∆Vbe   is applied externally (∆Vext  ) and the DS1925 ADC is next configured to measure internal Vbe   according to Equation 6.
 
ADC Code= ∆VextVbe+∆Vext Eq. (6)


However, relative to an ideal BJT diode characteristic that is required for operation of the temperature sensor circuit, due to wafer process variations this Vbe   has a temperature error and needs to be calibrated.  Shown in Figure 3 is the natural voltage (Vbe)  vs. temperature characteristic of a BJT diode under a constant current condition.  There are three Vbe   curves plotted: ideal, Vbe   with positive error, and Vbe   with negative error.  During this test step the uncalibrated Vbe   is obtained from equation 6 and an adjustment is performed to effectively move (i.e. calibrate) the measured Vbe  , positively or negatively as needed, to the ideal curve.  As noted previously, once Vbe   is calibrated to ideal at T  , it operates with the ideal characteristic across all temperatures.


Figure 3: Vbe   vs. Temperature

Verification

Calibrated units were swept in a temperature chamber across the -40C to +85C range. Figure 4 captures the data demonstrating a tight distribution of temperature measurement performance well within the +/-0.5C datasheet limits.



Figure 4: Calibrated DS1925 Temperature Accuracy

Conclusion

By using the known diode equations and applying precise external voltages during the calibration process, each of the unknown variables in the temperature equation can be solved to a) determine the DS1925 operating temperature at the calibration test step, and b) calibrate the diode Vbe   characteristics at this same test step to ideal. Once calibrated at this single test point, Vbe   provides a precise +/-0.5C accurate measurement of DS1925 operating temperature across the entire -40C to +85C range.















Sources
  1. https://en.wikipedia.org/wiki/Silicon_bandgap_temperature_sensor
  2. This adjustment of the Vbe   characteristic to ideal is a well-established electrical engineering principle within the domain of IC-based band-gap temperature sensor design.  Within the industry it is known as adjusting to the “Magic Voltage”.
Tags: Temperature Data Loggers calibration logger data process DS1925 KA-16575 Temperature Sensor and Control Devices mems inertial sensors Show More