Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Sensors
Sensors
Documents Why is the measured high pass filter corner frequency on the MAX30003 greater than expected?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • +AD5940: FAQ
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • +DS1922L-F5#: FAQ
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • +DS1925L-F5#: FAQ
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • +MAX30001CTI+T: FAQ
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • -MAX30003CTI+T: FAQ
    • Are INTB and INT2B open-drain in the MAX30003?
    • Do the MAX30003 FCLK and SCLK pins have internal ESD diodes between these pins and any of the VDD pins?
    • Does Maxim have any devices that implement the Pan-Tompkins algorithm?
    • ECG pole materilal
    • For the MAX30003, what amplitude of the ECG signal will cause clipping ?
    • How can we determine the resistance between ECGP and ECGN at which the MAX30003 will detect a DC Leads Off condition ?
    • How much ECG performance do I get when connecting a third electrode to VCM?
    • In the MAX30003, what is the equation to convert the ADC code to the ECG reading in volts?
    • Is any power sequencing required for the MAX30003?
    • Is there any layout guide for the MAX30003?
    • The input impedance of MAX30003 is very large, but how to keep the high input impedance for the system when we use dry electrodes?
    • The MAXREFDES100 schematic is different from that in the MAX30003 data sheet. Which one should I refer to?
    • What is the ECG noise histogram, and how can I read it?
    • What is the exact pin description in the MAX30003 datasheet for I.C. (internally connected) pins?
    • What is the main difference between the MAX30003 and the MAX30004?
    • Why is the measured high pass filter corner frequency on the MAX30003 greater than expected?
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • +MAX35103EVKIT#: FAQ
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

Why is the measured high pass filter corner frequency on the MAX30003 greater than expected?

The corner frequency of the high pass filter for MAX30003 is given by 

Fhp = 1/(2 x pi x Rhpf x Chpf),

where Rhpf is an internal resistance (typ value = 450kohm), and Chpf is the external capacitance connected between CAPP and CAPN. 

So with a 1.47uF (1uF + 0.47uF) capacitance between CAPP and CAPN, the expected  high pass filter corner frequency is 0.24Hz. 

However, with specific 1uF and 0.47uF capacitors, the actual measured high pass filter corner frequency was found to be 0.5Hz.

This happens because the effective value of the capacitance between CAPP and CAPN is smaller than the nominal value because of dc and ac derating. The ac and dc voltage of the input ECG signal directly appear across CAPP and CAPN, and must be accounted for when determining the HPF corner frequency. 

For example with a 1uF (nominal) cap with manufacturer part number CL03A105MQ3CSN, the ac and dc derating curves look as follows: 

 

Note that even if there is no dc bias in the input signal, since the ac signal amplitude of an ecg signal is very small, the effective capacitance value could be smaller than the nominal capacitance by 40%. 

Tags: hpf corner frequency high pass filter Biopotential Sensors ecg MAX30003 KA-06123 MAX30003CTI+ MAX30001 Bio-Sensors Show More