Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Sensors
Sensors
Documents For MAX30001 what is the equation that relates BioZ (impedance) to the ADC output in the BioZ FIFO?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • +AD5940: FAQ
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • +DS1922L-F5#: FAQ
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • +DS1925L-F5#: FAQ
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • -MAX30001CTI+T: FAQ
    • Can I miss to connect 1nF shunt-cap connected to CPLL of MAX30001 but directly connected CPLL to GND?
    • Does ECG/EKG feature required FDA certification approval?
    • Does the phase offset (BIOZ_PHOFF setting in MAX30001) impact overall performance (noise, in particular) in any way?
    • For MAX30001 what is the equation that relates BioZ (impedance) to the ADC output in the BioZ FIFO?
    • How could the MAX30001 AFE also be used to measure hydration?
    • How do I ensure that the ECG signals couple the same common node noise?
    • How do I optimize Maxim ECG AFE registers?
    • If there is a non-negligible parasitic capacitance to GND(~100pF) on dry electrodes before the EMI filters, are there any pressing concerns with this level of capacitance on the electrodes for both ECG and BIOZ?
    • In the MAX30001 BIOZ channel, what is the phase relationship between the Demodulator Signal and the Drive Current signal?
    • Is it possible to shift electrodes to the human body backside to measure ECG signals ?
    • Is there any reliable method, without using a different FCLK, to increase the BIOZ sampling rate to about 100Hz?
    • Should I split AGND and DGND in the MAX30001?
    • Should I use MAX30001 or MAX86150 as ECG AFE for DRY ELECTRODES?
    • What are the effects of each of the BMUX_CG_MODE settings, and should we be using the resistive CM setting (0b11) when biasing using the internal resistors?
    • What are the leads of ECG?
    • What are the voltage amplitudes for a human ECG?
    • What is a Holter Monitor?
    • What is HRV (Heart Rate Variability)?
    • What is pulse transit time (PTT)?
    • What is the dynamic range of MAX3000x ECG device?
    • What is the maximum impedance the MAX30001 can measure?
    • What MAX30001/MAX30003 register settings will eliminate the motion artifacts?
    • What type of capacitors are recommended for use with the MAX30001 to minimize the noise?
    • What would be a good algorithm to measure heart rate in a noisy environment with a lot of artifacts?
    • What's the frequency range of ECG analyzer made for China?
    • When will the MAX30001CTI+ (28 TQFN pkg) be available?
    • Why MAX30001/ECG signal input should be matched?
    • Why most Maxim's reference designs for ECG application have driving electrodes (Right leg drive)?
    • Why we need to connect a 1uF capacitor between CAPP and CAPN in MAX30001 design?
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • +MAX30003CTI+T: FAQ
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • +MAX35103EVKIT#: FAQ
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

For MAX30001 what is the equation that relates BioZ (impedance) to the ADC output in the BioZ FIFO?

BioZ Reading (ohm) = (VREF×[20 bit ADC code]) / (BioZ Drive current × 2^19 × BioZ Gain Setting)

Where VREF = 1V. BioZ Drive Current is programmable to 8uA, 16uA, 32uA, 48uA, 64uA, 80uA, or 96uA.  BioZ Gain Setting is programmable to 10, 20, 40, or 80 V/V .

The 20-bit ADC code is in two’s complement format so the right polarity needs to be considered when converting to decimal.

Tags: adc Biopotential Sensors MAX30001CTI+ KA-05590 equation MAX30001 bioz Bio-Sensors fifo scale Show More