• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Sensors
Sensors
Documents What are the effects of each of the BMUX_CG_MODE settings, and should we be using the resistive CM setting (0b11) when biasing using the internal resistors?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • +AD5940: FAQ
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • +DS1922L-F5#: FAQ
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • +DS1925L-F5#: FAQ
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • -MAX30001CTI+T: FAQ
    • Can I miss to connect 1nF shunt-cap connected to CPLL of MAX30001 but directly connected CPLL to GND?
    • Does ECG/EKG feature required FDA certification approval?
    • Does the phase offset (BIOZ_PHOFF setting in MAX30001) impact overall performance (noise, in particular) in any way?
    • For MAX30001 what is the equation that relates BioZ (impedance) to the ADC output in the BioZ FIFO?
    • How could the MAX30001 AFE also be used to measure hydration?
    • How do I ensure that the ECG signals couple the same common node noise?
    • How do I optimize Maxim ECG AFE registers?
    • If there is a non-negligible parasitic capacitance to GND(~100pF) on dry electrodes before the EMI filters, are there any pressing concerns with this level of capacitance on the electrodes for both ECG and BIOZ?
    • In the MAX30001 BIOZ channel, what is the phase relationship between the Demodulator Signal and the Drive Current signal?
    • Is it possible to shift electrodes to the human body backside to measure ECG signals ?
    • Is there any reliable method, without using a different FCLK, to increase the BIOZ sampling rate to about 100Hz?
    • Should I split AGND and DGND in the MAX30001?
    • Should I use MAX30001 or MAX86150 as ECG AFE for DRY ELECTRODES?
    • What are the effects of each of the BMUX_CG_MODE settings, and should we be using the resistive CM setting (0b11) when biasing using the internal resistors?
    • What are the leads of ECG?
    • What are the voltage amplitudes for a human ECG?
    • What is a Holter Monitor?
    • What is HRV (Heart Rate Variability)?
    • What is pulse transit time (PTT)?
    • What is the dynamic range of MAX3000x ECG device?
    • What is the maximum impedance the MAX30001 can measure?
    • What MAX30001/MAX30003 register settings will eliminate the motion artifacts?
    • What type of capacitors are recommended for use with the MAX30001 to minimize the noise?
    • What would be a good algorithm to measure heart rate in a noisy environment with a lot of artifacts?
    • What's the frequency range of ECG analyzer made for China?
    • When will the MAX30001CTI+ (28 TQFN pkg) be available?
    • Why MAX30001/ECG signal input should be matched?
    • Why most Maxim's reference designs for ECG application have driving electrodes (Right leg drive)?
    • Why we need to connect a 1uF capacitor between CAPP and CAPN in MAX30001 design?
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • +MAX30003CTI+T: FAQ
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • +MAX35103EVKIT#: FAQ
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

What are the effects of each of the BMUX_CG_MODE settings, and should we be using the resistive CM setting (0b11) when biasing using the internal resistors?

The reference to chopping is really a reference to the use of dynamic element switching; the use of which improves matching between the sink and source current sources.  The technique used for this dynamic switching also has the nice characteristic of reducing the magnitude of  1/f noise.  The reference to low pass filtering is the optional selection of an LPF within a common mode feedback circuit within the current generator that improves (i.e., increases) common mode input impedance when using a two-electrode solution (i.e., ECG and BioZ amplifiers and drive circuits use the same electrodes).  The final option eliminates the common mode feedback, and instead common-mode is established using two resistors. 

So, one can look at the four options as follows:

 

Mode 00: No chopping, thus higher 1/f noise. CFB with low-pass filter, thus high common-mode impedance at 50Hz and 60Hz

Mode 01: Chopping, thus almost no 1/f noise. CFB without low-pass filter, thus lower common-mode impedance at 50Hz and 60Hz

Mode 10: Chopping, thus almost no 1/f noise. CFB with low-pass filter, thus high common-mode impedance at 50Hz and 60Hz. Intuitively, this seems to be the best mode. However, due to the low bandwidth of the CMFB amplifier, stability of the CMFB loop is not guaranteed under all circumstances.

Mode 11: Chopping, thus almost no 1/f noise. No common-mode feedback; the common-mode is realized using two resistors. This mode has high common-mode impedance at 50Hz and 60Hz, but has lower input impedance than the CMFB amplifier, and may exceed the common-mode range for drive currents higher than 32uA due to mismatch.

 

We believe that the user can optimize for best matching and noise results for their particular application by selecting the option that works best for them.  Consider it a toolbox for optimizing the BioZ results.

Tags: Bio Impedance MAX30001CTI+ KA-03131 MAX30001 bioz BMUX_CG_MODE Show More