Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Sensors
Sensors
Documents Do third-party companies manufacture waterproof or water-resistant solutions for iButton data loggers?
  • Q&A
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • +AD5940: FAQ
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • -DS1922L-F5#: FAQ
    • Are Maxim's Temperature Logger iButtons NIST traceable?
    • Can ibuttons be ingested by animals or placed under the skin?
    • Do third-party companies manufacture waterproof or water-resistant solutions for iButton data loggers?
    • How to use OneWireViewer to set the password
    • ibutton clock synchronization
    • Magnetic iButton accessories
    • What is the thermal response time constant of the DS1922L?
    • What side of the iButton is the temperature sensor located?
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • +DS1925L-F5#: FAQ
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • +MAX30001CTI+T: FAQ
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • +MAX30003CTI+T: FAQ
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • +MAX35103EVKIT#: FAQ
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

Do third-party companies manufacture waterproof or water-resistant solutions for iButton data loggers?

Yes.  Here are some resources for making iButtonRegistered data loggers (Thermochrons) waterproof and/or using them in water or liquid monitoring applications:

  1. Maxim manufactures the DS9107 "iButton Capsule".  The iButtonRegistered Capsule is a mechanical enclosure to protect Temperature Logger iButtons (DS1921, DS1922, and DS1925 series) from moisture, solvents and pressure. It provides IP68 protection.  More info can be found here: https://www.analog.com/en/products/ds9107.html
  2. Homechip sells several waterproofing enclosures for iButton data loggers, including:  1 sinking silicon Thermochron enclosure, 1 floating silicon enclosure, and 1 aluminum half-enclosure:  https://homechip.com/search?type=product&q=data+logger+enclosure
  3. For Do-It-Yourself (DIY) waterproofing Thermochron solutions, there has been a published study on the efficacy of coating iButton devices with clear plastic dip: https://www.researchgate.net/publication/257160340_Does_waterproofing_Thermochron_iButton_dataloggers_influence_temperature_readings

 

 

Tags: Temperature Data Loggers solutions data loggers DS9107 KA-01737 iButton Mounting Options DS1922 iButton Devices and Accessories Thermochrons waterproof waterproofing DS1925 DS1921 DS1922L-F5# data logger Temperature Sensor and Control Devices iButton water resistant Thermochron Show More
  • Share
  • History
  • Cancel
 
Related Content
  • ibutton
    ibutton
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • Can you retrieve data from an iButton that is no longer being recognized or is dead?
    MSDAPI
    Maxim makes quite a few iButton devices. Some of these don't require batteries, but several do. Unfortunately when an iButton battery dies, the data stored in the memory is lost. The only exception to...
  • Does the iButton temperature sensor measure surface temperature or air temperature?
    MSDAPI
    In the iButton temperature sensor, the physical location of the temperature sensor is in the middle of the iButton. The circuit board and battery are closer to the side of the iButton with a flange and...
 
Related Content
  • ibutton
    ibutton
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • Can you retrieve data from an iButton that is no longer being recognized or is dead?
    MSDAPI
    Maxim makes quite a few iButton devices. Some of these don't require batteries, but several do. Unfortunately when an iButton battery dies, the data stored in the memory is lost. The only exception to...
  • Does the iButton temperature sensor measure surface temperature or air temperature?
    MSDAPI
    In the iButton temperature sensor, the physical location of the temperature sensor is in the middle of the iButton. The circuit board and battery are closer to the side of the iButton with a flange and...