Upcoming Webinar: Simplify High-Accuracy Instrumentation Design with Latest Precision Data Converters

    Join us for an insightful webinar on how ADI’s Precision technology is transforming the landscape of high accuracy instrument design with cutting-edge...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    Exploring DCM and CCM in SMPS: Part 1 of 6

    Power supplies are the unsung heroes of electronic devices, ensuring that they receive the precise, stable, and clean DC voltages they need to function...

     

    Let’s Take a Field-Bus Trip

    Let’s dive deep into what makes field buses unique compared to each other. Building on our previous blog post, What Makes Field Bus Communication Unique...

    Latest Blogs

    • Countable vs Non-countable Faults
    • Power Your Signal: DAS Networks Unleashed: Part 2 of 4
    • Combining Functional Safety and Availability Using Redundancy
    • Top 3 Engineering Blogs That Captivated Minds on EngineerZone
    • How to Generate a Custom Profile for Optimal System Performance
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
Temperature Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Temperature Sensors
Temperature Sensors
Documents AD59x Correct Thermocouple Grounding
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • More
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • -AD5940: FAQ
    • AD594 AD595 for N type thermocouple
    • AD594: ESD and EMI protection
    • AD594: Type T thermocouple
    • AD594: Voltage changews with supply voltage
    • AD59x Correct Thermocouple Grounding
    • AD59x Output Value not close to Expected Value
    • Keil requires Compiler Version 5 to use the AD594x sample code, where can I find this version?
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • +DS1922L-F5#: FAQ
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • +DS1925L-F5#: FAQ
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • +MAX30001CTI+T: FAQ
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • +MAX30003CTI+T: FAQ
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • +MAX35103EVKIT#: FAQ
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

AD59x Correct Thermocouple Grounding

Question

I do not understand how to correctly ground my thermocouple?

Answer

When using the AD59x, the thermocouple should be grounded at one place, and
only one
place. The grounding can occur at the negative input of the AD59x, the positive
input of
the AD59x, or at the thermocouple tip.
Where the thermocouple is grounded will change the behaviour of the AD59x
during an
open thermocouple condition. If the negative input is grounded, the part’s
output voltage
will rail high during an open thermocouple event. If the positive input is
grounded, the
part’s output voltage will rail low during an open thermocouple event.
Behaviour is
undefined if grounding at the thermocouple tip.
Special Case: Non-isolated thermocouples
For good measurements, it is critical to only have one ground point. The vast
majority of
thermocouples have an electrically isolated sheath around the sensing end, so
there is no
electrical contact between the material being sensed and the thermocouple.
However
some types of thermocouples (such as those designed to respond very quickly)
may allow
an electrical connection between the material being measured and the
thermocouple. In
this case, if the material being measured is grounded, this connection counts
as the
thermocouple’s “ground” and the AD59x should not be grounded at one of the
input pins.
With long thermocouple connections the “ground” at the tip may be considerably
different than the ground at the AD59x. In these cases it is recommended to run
the
AD59x with a dual supply, so that if the “ground” at the thermocouple deviates
somewhat from the AD59x’s ground, it will still be in the common mode range of
the
part.

Tags: 3AUS1758 temperature sensors ad594