Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ296 about repairing an equation in a digital display

      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Sensors
Sensors
Documents What are the differences between the two MAX35103 EVKITs?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD22100: FAQ
  • +AD22151G: FAQ
  • +AD580: FAQ
  • +AD581SH: FAQ
  • +AD584: FAQ
  • +AD590: FAQ
  • +AD590JF: FAQ
  • +AD590S: FAQ
  • +AD592C: FAQ
  • +AD5940: FAQ
  • AD594: FAQ
  • +AD595: FAQ
  • +AD595AQ: FAQ
  • +AD597: FAQ
  • +ad7414: FAQ
  • +AD8495: FAQ
  • +ADAS1000: FAQ
  • +ADIS16003: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADT70: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7411: FAQ
  • +ADT7420: FAQ
  • +ADT7422: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +adt7470: FAQ
  • +ADUCM355: FAQ
  • +ADXL00125: FAQ
  • +ADXL103: FAQ
  • +ADXL193: FAQ
  • +ADXL202: FAQ
  • +ADXL203: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL213: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL326: FAQ
  • +ADXL327: FAQ
  • +ADXL330: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +ADXL346: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL363: FAQ
  • +ADXL372: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADXRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +DS1921G-F5#: FAQ
  • +DS1921G: FAQ
  • +DS1921H-F5#: FAQ
  • +DS1922E-F5#: FAQ
  • DS1922E: FAQ
  • +DS1922L-F5#: FAQ
  • +DS1923-F5#: FAQ
  • +DS1923-F5+: FAQ
  • +DS1925L-F5#: FAQ
  • +DS600: FAQ
  • +EVAL-ADXL313-SDP: FAQ
  • LM26: FAQ
  • +LTC298x Family FAQs
  • MAX30001CTI+: FAQ
  • +MAX30001CTI+T: FAQ
  • +MAX30001CWV+: FAQ
  • +MAX30001EVSYS#: FAQ
  • +MAX30001GCWV+: FAQ
  • +MAX30001GEVKIT#: FAQ
  • +MAX30001_TI+_A1: FAQ
  • +MAX30002CTI+: FAQ
  • MAX30003: FAQ
  • +MAX30003CC/D+: FAQ
  • MAX30003CTI+: FAQ
  • +MAX30003CTI+T: FAQ
  • +MAX30003WING#: FAQ
  • +MAX30009: FAQ
  • +MAX30131CWA+: FAQ
  • +MAX30134CWA+: FAQ
  • +MAX30134EVSYS#: FAQ
  • MAX30205: FAQ
  • +MAX30205EVKIT#: FAQ
  • +MAX30205EVSYS#: FAQ
  • +MAX30205MTA+T: FAQ
  • MAX30208CLB+: FAQ
  • +MAX30208CLB+_T1: FAQ
  • +MAX30208_LB+_A1: FAQ
  • MAX35101: FAQ
  • +MAX35101EHJ+: FAQ
  • MAX35102: FAQ
  • +MAX35102ETJ+: FAQ
  • +MAX35103EHJ+: FAQ
  • -MAX35103EVKIT#: FAQ
    • Can MAX35103 EVKIT be connected to the MCU board of the user for testing?
    • How do I convert the TOF measured by MAX35103 to flow rate?
    • How to change and reset the Alarm Function in the MAX35103?
    • Is the MAX35101EVKIT default configuration file also compatible with the MAX35103EVKIT?
    • We have purchased a MAX35103evkit to get an idea producing an ultrasonic flow meter using MAX35103. As we are using 2Mhz piezo sensor with it. How can we configure 2MHz sensor with the kit?
    • What are some things to check if the crystal on the MAX35103 is not starting up?
    • What are the differences between the two MAX35103 EVKITs?
    • Why is the time measurement accuracy specification in the EC table of MAX35101, MAX35102, MAX35103 typically 20 ps while the absolute ToF Error in TOCs are in the order of tens of nanoseconds?
  • MAX35103EVKIT: FAQ
  • MAX35104ETL+: FAQ
  • +MAX35104ETL+T: FAQ
  • +MAX35104EVKIT2#: FAQ
  • +MAX6510HAUT+: FAQ
  • +MAX6517: FAQ
  • MAX6607: FAQ
  • +MAX6675ISA+: FAQ
  • MAX6675ISA: FAQ
  • +MAX86160: FAQ
  • +MAX9924UAUB+: FAQ
  • +MAX9925: FAQ
  • +Temperature sensor: FAQ
  • +TMP01: FAQ
  • +TMP35: FAQ

What are the differences between the two MAX35103 EVKITs?

There are two different evaluation kits for the MAX35103: the MAX35103EVKIT# and the MAX35103EVKIT2#.  While they both include the MAX35103, the features of the EVKITs are different.

The MAX35103EVKIT# comes with a PC software tool designed to help you configure the chip for your own flow meter hardware.  The board is highly configurable, and it should be used to evaluate the MAX35103 for a specific application. 

The MAX35103EVKIT2# is an application example intended as an off-the-shelf flow-metering solution.  That said, it can be useful as a prototyping platform for some applications, but it is not nearly as configurable as the MAX35103EVKIT#.  You can program the micro on this kit via JTAG, but it will not work with the PC software tool used with the MAX35103EVKIT#.  The MAX35103EVKIT2# comes with pre-loaded firmware for flow-metering.
Tags: 000099477 MAX35103 temperature sensors