Hi,
I already programmed a microcontroller to use adt7301. Can I use the same code to adt7311?
ADT7301
Production
The ADT7301 is a complete temperature monitoring system in SOT-23 and MSOP packages. It contains a band gap temperature sensor and a 13-bit ADC to monitor...
Datasheet
ADT7301 on Analog.com
ADT7311
Recommended for New Designs
The ADT7311 is a high accuracy digital temperature sensor in a narrow 8-lead SOIC package. It contains a band gap temperature reference and a 16-bit ADC...
Datasheet
ADT7311 on Analog.com
Hi,
I already programmed a microcontroller to use adt7301. Can I use the same code to adt7311?
Hi,
You need to write a new code for the ADT7311. The ADT7311 has additional features like open drain output pins, modes and registers not on the ADT7301, and different timing specs.
Regards,
Karen