Hi All,
Before building up my temperature measurement system (PC--DC2026--DC2209--DC2212) , I have a couple of questions. Please take care of this case.
Q1 and Q2 : Please refer to the attachment.
Q3: Are there any settings and/or adjustments to LTC2983 before temperature measurement?
Q4: I'm going to start our trial production if the demo system works well. In that case you can provide any helpful software?
Regards,
Kazu
Hi Logan,
About the way to speed up by using two LTC2986s, how can I get 12ch in 1s since this part's ODR is 164ms typ in the two conversion cycle mode?
About the bootloader, sorry I will check with our SW engineer.
About taking measures for latch-up, LTC2983 and LTC2983 do not need such protection or do you recommend to prepare a current limiting resistor along with a low-leakage TVS?