AD590 Moisture Sensitivity Level

What is the MSL level for the various AD590 packages?

  • The AD590 MSL rating depends on the package in question:

    For AD590 8-ld SOIC, MSL rating = 1.

    For AD590 2-ld CQFP and 3-pin T0-52, MSL rating = N/A

    For the 2-ld CQFP and 3-pin T0-52 packages, both are housed in a ceramic hermetically sealed package. Because the die is not encapsulated with plastic (and therefore does not absorb moisture) it's not affected by moisture in the same way as a plastic package so therefore does not have an MSL rating.

  • 0
    •  Analog Employees 
    on Apr 29, 2019 10:38 AM
    This question has been closed by the EZ team and is assumed answered.