Hi,
We are using two ADT6401 temperature switches on our board. They are open-drain output. We use one for the high temperature (+85 degrees celcius) and one for the low temperature (-45 degrees celcius). Our schematic is attached.
Temperature switches can shutdown our board. While we are testing the board at room temperature, our board shuts down because one of the temperature switches pulls their output low. We could not understand which of them. But the temperature is very far away from both high and low limits. So temperature switches do not operate correctly, that's for sure.
Our low temp. switch inputs are Float - GND - Float. If the float on the S2 pin, is measured as GND some time, the temperature setting goes to +65 degrees celcius. Could this be a problem? Or could it be a soldering effect?
Thanks,
Celil
I am mallikarjun from honeywell. We are planning to use this component in one of our new design. Whether this dependency on VCC Rise time (2.5ms upto 0 to 2.7V) is still existing for this part. Any device errata/ whether this problem rectified in latest part (ADT6401)?
Whether same problem exists form ADT6402 also?
My email: malli.koppanati@honeywell.com
+91 8095950458