Post Go back to editing

ADT6401 Output Problem

Thread Summary

The user is experiencing incorrect operation of ADT6401 temperature switches on their board, which shut down the board at room temperature. The issue is due to the part not entering the correct mode when the Vcc rise time is greater than 10ms, causing floating inputs to be misinterpreted as GND. The user tested the ADT6401 and found that it checks its inputs 2.5ms after power-up, leading to incorrect latching of input states with slow Vcc rise times. A potential alternative is the ADT6501, which has factory-set trip points in a similar package.
AI Generated Content

Hi,

We are using two ADT6401 temperature switches on our board. They are open-drain output. We use one for the high temperature (+85 degrees celcius) and one for the low temperature (-45 degrees celcius). Our schematic is attached.


Temperature switches can shutdown our board. While we are testing the board at room temperature, our board shuts down because one of the temperature switches pulls their output low. We could not understand which of them. But the temperature is very far away from both high and low limits. So temperature switches do not operate correctly, that's for sure.

Our low temp. switch inputs are Float - GND - Float. If the float on the S2 pin, is measured as GND some time, the temperature setting goes to +65 degrees celcius. Could this be a problem? Or could it be a soldering effect?

Thanks,


Celil

Parents
  • Hi, apologies for delay in getting back. We have looked at ADT6401 on the bench and when the rise time is >10mS from 0->2.7V, the part isn’t entering the correct mode with the associated floating inputs.

    We also tied the S2 & S0 pins to Vdd/2 but to no avail as part interprets the pins as a high.

    The next nearest family is ADT6501, these have factory set trip points in a similar SOT23 package.

Reply
  • Hi, apologies for delay in getting back. We have looked at ADT6401 on the bench and when the rise time is >10mS from 0->2.7V, the part isn’t entering the correct mode with the associated floating inputs.

    We also tied the S2 & S0 pins to Vdd/2 but to no avail as part interprets the pins as a high.

    The next nearest family is ADT6501, these have factory set trip points in a similar SOT23 package.

Children
  • Are there plans to add this minimum supply voltage slew rate information to the datasheet or plans to better define how the IC detects "floating" pins? I have boards with the ADT6401 that are failing to trip at cold temperature because we need a slow supply voltage ramp. We could have saved a lot of time debugging and redesigning if this was in the datasheet instead of only in a forum post. It's unfortunate that all of the cold trip setting require at least 1 floating pin.

    The ADT6503/ADT6504 would have been good cold-trip substitutes if they were still in production. We are looking into using MAX6503 chips instead.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.