Post Go back to editing

ADT6401 Output Problem

Hi,

We are using two ADT6401 temperature switches on our board. They are open-drain output. We use one for the high temperature (+85 degrees celcius) and one for the low temperature (-45 degrees celcius). Our schematic is attached.


Temperature switches can shutdown our board. While we are testing the board at room temperature, our board shuts down because one of the temperature switches pulls their output low. We could not understand which of them. But the temperature is very far away from both high and low limits. So temperature switches do not operate correctly, that's for sure.

Our low temp. switch inputs are Float - GND - Float. If the float on the S2 pin, is measured as GND some time, the temperature setting goes to +65 degrees celcius. Could this be a problem? Or could it be a soldering effect?

Thanks,


Celil

Parents
  • Hi,

    We use LDO for the supply so we cannot control the risetime.

    Is there anything we can do, to make the FLOAT pins appear correctly with the slow rise time?

    If not, is there any alternate parts that is pin compatible or same package?

    If there is nothing we can do, we have to cancel these parts.

    Celil

Reply
  • Hi,

    We use LDO for the supply so we cannot control the risetime.

    Is there anything we can do, to make the FLOAT pins appear correctly with the slow rise time?

    If not, is there any alternate parts that is pin compatible or same package?

    If there is nothing we can do, we have to cancel these parts.

    Celil

Children
No Data