Post Go back to editing

ADT6401 Output Problem

Thread Summary

The user is experiencing incorrect operation of ADT6401 temperature switches on their board, which shut down the board at room temperature. The issue is due to the part not entering the correct mode when the Vcc rise time is greater than 10ms, causing floating inputs to be misinterpreted as GND. The user tested the ADT6401 and found that it checks its inputs 2.5ms after power-up, leading to incorrect latching of input states with slow Vcc rise times. A potential alternative is the ADT6501, which has factory-set trip points in a similar package.
AI Generated Content

Hi,

We are using two ADT6401 temperature switches on our board. They are open-drain output. We use one for the high temperature (+85 degrees celcius) and one for the low temperature (-45 degrees celcius). Our schematic is attached.


Temperature switches can shutdown our board. While we are testing the board at room temperature, our board shuts down because one of the temperature switches pulls their output low. We could not understand which of them. But the temperature is very far away from both high and low limits. So temperature switches do not operate correctly, that's for sure.

Our low temp. switch inputs are Float - GND - Float. If the float on the S2 pin, is measured as GND some time, the temperature setting goes to +65 degrees celcius. Could this be a problem? Or could it be a soldering effect?

Thanks,


Celil

Parents
  • Hi again,

    - There are 100nF caps very close to the IC's (one for each).

    - The output is pulled high to 4 volts with 100 uA current.

    To isolate the problem, we did some tests to the ADT6401 in a test board and we think we isolated the problem. Below are our findings:

    In the datasheet, ADT6401's operating supply voltage is given as 2,7 volts.

    1) 2,5 ms after powerup, ADT6401 checks its inputs (whether they are float, gnd, or Vcc)

    2) ADT6401 checks its inputs once and only once (2,5 ms after powerup).

    3) So, if anything goes wrong at powerup, the input states are latched.

    4) If Vcc rises slowly (1 volts per 25 ms), the float pins is not read correctly. They are read as GND's.

    So, in our case,

    S2/S1/S0 (Float-GND-Float) (-45 degrees with 2 degrees hysteresis) becomes

    S2/S1/S0 (GND-GND-GND) (+45 degrees with 2 degrees hysteresis).

    We tested ADT6401 for 2 full days. We tested with scope. We know it checks its inputs 2,5 ms after powerup, because we measured the FLOAT pin and saw that it rises to half of Vcc 2,5 ms after powerup.

    That is very critical for us. We need to make sure that ADT6401 reads FLOAT state correctly independent of the rise time of Vcc.

    Please reply ASAP.

    Thanks and sincerely,

    Celil

Reply
  • Hi again,

    - There are 100nF caps very close to the IC's (one for each).

    - The output is pulled high to 4 volts with 100 uA current.

    To isolate the problem, we did some tests to the ADT6401 in a test board and we think we isolated the problem. Below are our findings:

    In the datasheet, ADT6401's operating supply voltage is given as 2,7 volts.

    1) 2,5 ms after powerup, ADT6401 checks its inputs (whether they are float, gnd, or Vcc)

    2) ADT6401 checks its inputs once and only once (2,5 ms after powerup).

    3) So, if anything goes wrong at powerup, the input states are latched.

    4) If Vcc rises slowly (1 volts per 25 ms), the float pins is not read correctly. They are read as GND's.

    So, in our case,

    S2/S1/S0 (Float-GND-Float) (-45 degrees with 2 degrees hysteresis) becomes

    S2/S1/S0 (GND-GND-GND) (+45 degrees with 2 degrees hysteresis).

    We tested ADT6401 for 2 full days. We tested with scope. We know it checks its inputs 2,5 ms after powerup, because we measured the FLOAT pin and saw that it rises to half of Vcc 2,5 ms after powerup.

    That is very critical for us. We need to make sure that ADT6401 reads FLOAT state correctly independent of the rise time of Vcc.

    Please reply ASAP.

    Thanks and sincerely,

    Celil

Children
No Data