Post Go back to editing

The resistance of pin(+)-Pin(-) AD592

Dear Sir/Madam,


Our customer found the bad resistance AD592 of between pin(+) to pin(-) in their acceptance inspection.

The way of inspection is to use DMM.

1; The stick ( + ) of DMM put on your pin( +).

2; The stick ( -) of DMM put on your pin( -).

3; Measure the resistance, the result is 28Mohm.

5; The stick ( + ) of DMM put on your pin( -).

6; The stick ( -) of DMM put on your pin( +).

7; Measure the resistance, the result is infinity.

This is no problem but he found some sample that the result step-7 was 450kohm.


Your AD592 internal block have current source I know.

DMM will send small voltage from stick( +).


1)Please advice us why above 450kohm result comin? I could not find your internal circuit on you datasheet.

2)Is the above 450kohm AD592 defective?or not?

3)Is the above inspection way no prpblem? Or do you have a good inspection way?

  I think that he should add the 5V on pin( +)  ,put the 10kohm resister on pin( -) to GND, and measure the voltage on both end of the resister.

 

Thanks Kaos


Parents
  • Hi Karen,

    Exactly, we should do the check as following way from your datasheet Fig-4,page 5 I believe.

    > I think that he should add the 5V on pin( +)  ,put the 10kohm resister on pin( -) to GND, and measure the voltage on both end of the resister.


    And we should confirm the checked data by Fig-1,page-4 also I believe.

    I said this to customer strongly.


    DMM push out the voltage from stick(+ ) around 1-3V I think.

    So in Fig-1, the add voltage 1-3V bring the unstable current from AD592.

    DMM measured the automatic mode maybe. If so, the unstable current make change unstable for the display at threshold.


    Is this correct????


    Kaos

Reply
  • Hi Karen,

    Exactly, we should do the check as following way from your datasheet Fig-4,page 5 I believe.

    > I think that he should add the 5V on pin( +)  ,put the 10kohm resister on pin( -) to GND, and measure the voltage on both end of the resister.


    And we should confirm the checked data by Fig-1,page-4 also I believe.

    I said this to customer strongly.


    DMM push out the voltage from stick(+ ) around 1-3V I think.

    So in Fig-1, the add voltage 1-3V bring the unstable current from AD592.

    DMM measured the automatic mode maybe. If so, the unstable current make change unstable for the display at threshold.


    Is this correct????


    Kaos

Children
No Data