Post Go back to editing

Which Thermocouple type to use with 5B47 for -100C to 300C

Thread Summary

The user is building an application to measure air temperatures between -100°C to 300°C using the 5B47 Isolated, Linearized Thermocouple Input. Despite the 5B47's highest accuracy with type J thermocouples, type J is not suitable for temperatures below 0°C due to condensation and rust concerns. Type T thermocouples are recommended for this temperature range, offering better low-temperature performance.
AI Generated Content

I am building an application to measure air temperatures between -100 deg C to 300 deg C.  I'm considering using the  5B47 Isolated, Linearized Thermocouple Input from AD.  The spec sheet for the 5B47 says that the highest accuracy for this temperature range is available from a type J thermocouple.  (+/- 0.5 deg C accuracy).  However, all the thermocouple manufacturers I have looked at say type J is not rated for temperatures below 0 deg C.  They all recommend type T thermocouples.  What am I missing?  Should I use type J or type T?

  • Hi seanengtxct,


    I'm not very familiar with the 5B47, but generally speaking, type J thermocouples are not used to measure temperatures below ambient due to concerns about condensation forming on the wires, which can cause the iron to rust. Type T thermocouples are good for cryogenic and laboratory applications where low temperatures are needed and the higher temperature range of type J is not needed. It sounds to me like type T would fit your measurement temp range very well, and personally I would choose type T despite the slightly lower accuracy of the module.


    Thanks,

    Scott

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.