AD7415 Absolute Maximum Ratings 

Hi all,

Here is the Absolute Maximum Ratings in the datasheet at AD7415,
SDA Input Voltage to GND : −0.3 V to +7 V
SCL Input Voltage to GND : −0.3 V to +7 V

This means that SDA & SCL are not related to VDD ?

"−0.3 V to VDD + 0.3 V" is correct ?
If VDD is off and host or others input to SDA & SCL,
is that no damege to SDA & SCL?

Best regards,
sss