Greetings,
when using the GPIO0 and GPIO1 outputs of ADPD1080/1081 are the outputs clamped to the DVDD? I.e. then setting GPIO0_ENA to '1' and GPIO0_DRV to '1' and pulling the GPIO0 to 3.3 volts with an external pull-up, will the logic high be DVDD - Vclamp (1.8V - 0.5V approximately), not 3.3 volts?
Thanks!