AD5940
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5940 on Analog.com

We have been testing the AD5940 using the EVAL-AD5940BIOZ board paired with EVAL-ADICUP3029. Our goal is to simulate one of our experimental conditions where electrode contact impedances are high, while the sensing impedance is as low as 10 Ω.
Using SensorPal, we selected the 4-Wire Impedance application, which successfully reported approximately 13 Ω, as expected. We also verified the excitation and sensing behavior by monitoring the CE0–AIN1 electrodes with an Analog Discovery oscilloscope. However, SensorPal does not allow frequency sweeps below 100 Hz, which is critical for our application. Below are the key parameters used in SensorPal:




Firmware Testing
To explore lower frequencies, I downloaded Keil µVision and the example codes from the official GitHub repository.
Impedance Example
/* Set switch matrix to onboard(EVAL-AD5940ELECZ) dummy sensor. */
pImpedanceCfg->DswitchSel = SWD_CE0;
pImpedanceCfg->PswitchSel = SWP_RE0;
pImpedanceCfg->NswitchSel = SWN_SE0;
pImpedanceCfg->TswitchSel = SWT_SE0LOAD;
/* The dummy sensor is as low as 5kOhm. We need to make sure RTIA is small enough that HSTIA won't be saturated. */
pImpedanceCfg->HstiaRtiaSel = HSTIARTIA_5K;
pImpedanceCfg->DswitchSel = SWD_CE0;
pImpedanceCfg->PswitchSel = SWP_CE0;
pImpedanceCfg->NswitchSel = SWN_AIN1;
pImpedanceCfg->TswitchSel = SWT_AIN1;
/* The dummy sensor is as low as 5kOhm. We need to make sure RTIA is small enough that HSTIA won't be saturated. */
pImpedanceCfg->HstiaRtiaSel = HSTIARTIA_200;
/* Configure the sweep function. */
pImpedanceCfg->SweepCfg.SweepEn = bTRUE;
pImpedanceCfg->SweepCfg.SweepStart = 100.0f; /* Start from 100Hz */
pImpedanceCfg->SweepCfg.SweepStop = 1000.0f; /* Stop at 1kHz */
pImpedanceCfg->SweepCfg.SweepPoints = 100; /* Points is 100 */
pImpedanceCfg->SweepCfg.SweepLog = bTRUE;
/* Configure Power Mode. Use HP mode if frequency is higher than 80kHz. */
pImpedanceCfg->PwrMod = AFEPWR_LP;
/* Configure filters if necessary */
pImpedanceCfg->ADCSinc3Osr = ADCSINC3OSR_2; /* Sample rate is 800kSPS/2 = 400kSPS */
pImpedanceCfg->DftNum = DFTNUM_16384;
pImpedanceCfg->DftSrc = DFTSRC_SINC3;
.PswitchSel = SWP_CE0,
.NswitchSel = SWN_AIN1,
.TswitchSel = SWT_AIN1,
.PwrMod = AFEPWR_LP,
.HstiaRtiaSel = HSTIARTIA_200,
.ExcitBufGain = EXCITBUFGAIN_2,
.HsDacGain = HSDACGAIN_1,
.HsDacUpdateRate = 7,
.DacVoltPP = 600.0,
.BiasVolt = -0.0f,
.SinFreq = 100.0, /* 100Hz */
.DftNum = DFTNUM_16384,
.DftSrc = DFTSRC_SINC3,
.HanWinEn = bTRUE,
.AdcPgaGain = ADCPGA_9,
.ADCSinc3Osr = ADCSINC3OSR_4,
.ADCSinc2Osr = ADCSINC2OSR_22,
.ADCAvgNum = ADCAVGNUM_16,
.SweepCfg.SweepEn = bTRUE,
.SweepCfg.SweepStart = 100,
.SweepCfg.SweepStop = 1000.0,
.SweepCfg.SweepPoints = 100,
.SweepCfg.SweepLog = bFALSE,
.SweepCfg.SweepIndex = 0,

BIA Example
.PwrMod = AFEPWR_LP,
.HstiaRtiaSel = HSTIARTIA_200,
.CtiaSel = 16,
.ExcitBufGain = EXCITBUFGAIN_2,
.HsDacGain = HSDACGAIN_1,
.HsDacUpdateRate = 7,
.DacVoltPP = 600.0,
.SinFreq = 100.0, /* 100Hz */
.ADCPgaGain = ADCPGA_9,
.ADCSinc3Osr = ADCSINC3OSR_4,
.ADCSinc2Osr = ADCSINC2OSR_22,
.DftNum = DFTNUM_16384,
.DftSrc = DFTSRC_SINC3,
.HanWinEn = bTRUE,
.SweepCfg.SweepEn = bTRUE,
.SweepCfg.SweepStart = 100,
.SweepCfg.SweepStop = 1000.0,
.SweepCfg.SweepPoints = 100,
.SweepCfg.SweepLog = bTRUE,
.SweepCfg.SweepIndex = 0,

At this point, I would appreciate your guidance on the following:
Hi,
BIA is 4-wire impedance measurement technique.
Sensorpal and Github code are exactly same except that Sample rate is limited to 10sps in Sensorpal, whereas in Github code, it is set by pBIACfg->BiaODR
Is you Sensorpal config same as you have set in Github code: