Post Go back to editing

aducm355 rtd temperature value shows wrong value

Category: Software
Product Number: aducm355

Hi Analog Team,

I am using ADUCM355(CN0428) and trying to read PT100 RTD sensor.First i connected 30kΩ resistor which read back a 25.3°C read in NTC mode.Then I changed code to RTD mode and read temperature it read back 35Ω and -250°C.Please give a solution as soon as possible.My project is on hold because of his issue.

  • When i connect a 4.7M resistor in conductivity channel and connect an RTD sensor in temperature the readings of temperature are changing drastically which can be seen in the document attached.When i connect 100Ω reisistor in RTD channel and the conductivity channel is left open the temperature is correct.when i connect resistor in both the channels issue arrises.Please give me a solution for this issue.
    PDF