Post Go back to editing

no support for Windows 11 1-wire on laptops running ARM64 (Snapdragon X Elite).

Thread Summary

The user encountered issues with the 1-wire driver for Thermochron data loggers on new Samsung laptops with ARM64 processors running Windows 11 Pro. The driver, last updated in 2009, is incompatible with ARM64. The user inquired if Analog Devices plans to update the USB driver to support ARM64 processors.
AI Generated Content
Category: Software
Product Number: DS1922L
Software Version: USB 1 wire drivers for Windows 4.05 (4.10)

Hi. 

I have already reached out to Analog on this issue but didn't get any timeline for when I would be addressed.

We are a long-time developer of the Thermochron data loggers using 1-wire, with more than 20+ years of experience with these devices.

Recently, a customer had issues installing our graphing analysis software on 2 Samsung laptops.

On investigation we found that the 1-wire driver could not be loaded by the system (was running Win11 Pro)

The customer had 2 new identical Samsung Laptops, both machines had the same problem.

I remoted into the machine and after a little head rubbing, noticed it was an ARM64 (Snapdragon X Elite) processor.

Now, the 1-wire driver has not been updated since 2009. So there's no chance for the driver to work, it probably needs to be re-compiled using the ARM processor resources.

The customers machines are Galaxy Book4  Edge, and the system info from that machine is in the image below.

I have looked at HP and DELL  both are offering ARM64-PC running Windows 11 now.  They give significantly improved battery life compared to Intel x64.

Looking around, there is an expectation that ARM64 will take 50% of the Laptop market within 5 years. (maybe?)

So, does anyone know if Analog are updating the USB driver? or are they happy to let this production line disappear into the oblivion?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.