Hello,
I have configured the channels on my LTC2983 for sense resistors and thermistors. I would like to verify that these channels are configured correctly by performing a READ on each channel assignment location (0x200 - 0x24F). However, the READ results are not as expected due to the following:
- A READ on the channel assignment memory locations (0x200 - 0x24F) always returns the most recent uint32_t that was written to memory, regardless of which channel assignment is being read.
- However, I can correctly read 0x40 from the command status register as expected.
- The same issue arises when I try to read from the custom Steinhart-Hart data locations (0x250 - 0x3CF).
My question is: Is this expected behavior? Does the user not have READ access in certain memory locations of the LTC2983?
Thanks for any help!