Good morning,
I am working for the first time with an AD5940 that I intend to use to make two-terminal impedance measurements on liquids. The AD5940 is mounted on a custom PCB with a 10 kOhm Rcal and I am making a measurement at 15kHz.
I am using the example codes provided by AD to make the impedance phase and magnitude measurement and am comparing the results with a simulation and calculations.
To test the accuracy of the system I am connecting components (example known resistor) and measuring their impedance.
PROBLEM: when I simply measure the impedance of the resistor the measurement is correct and coincides with the calculated value, however, if I add a capacitor in parallel to the resistor a or simply a capacitor directly connected to F+ and F- the measured phase is totally wrong for example: expected phase: -11.8°, measured phase -170°.
Currently I have not yet been able to understand the origin of the problem but I think it could be a problem in the software configuration of the AD5940, would you have any advice?
Thank you very much.