| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | mark.ramos DanB mkhairy RGrau Akila |
Open |
AD5941
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5941 on Analog.com
AD5940
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5940 on Analog.com
AD8233
Recommended for New Designs
The AD8233 is an integrated signal conditioning block for electrocardiogram (ECG) and other biopotential measurement applications. It is designed to extract...
Datasheet
AD8233 on Analog.com
AD8421
Recommended for New Designs
The AD8421 is a low cost, low power, extremely low noise, ultralow bias current, high speed instrumentation amplifier that is ideally suited for a broad...
Datasheet
AD8421 on Analog.com
Referring to this question:
is there way to use ad5940 without interrupt or GPIO interrupt pin?
I'm not sure if the author ever got it to work, anyway, so I have a requirement to generate the sinewave of programmable freq continuously in BIA setup (4 wire setup), and continuously get the ADC data, not stopping ever, till I manually stop it.
The current BIA example uses a sequencer, and the WG stops and starts all the time, as I cheded on the oscilloscope. I'm okay with the interrupt to trigger to notify if the data is ready, but not sure if I should use the sequencer? I tried to write the example myself without the sequencer, but it didn't work, and hence I'm here asking for help.
So, here's a question: Can AD594x continuously and simultaneously generate a sine wave and process the data via ADC? if yes, can I have the code in BIA formation, please?
Hi,
You may just remove the sleep command from all sequences in BIA code.
That is remove the below line wherever it is called:
AD5940_EnterSleepS();
Also inside measure sequence, WG block is turned off. You may remove the red part below:
AD5940_AFECtrlS(AFECTRL_ADCCNV|AFECTRL_DFT|AFECTRL_WG|AFECTRL_ADCPWR, bFALSE); /* Stop ADC convert and DFT */

Thanks for the reply. I implemented the changes, however, the WG stops/starts frequently, please see the attached screenshot. Could you share the code that you got it to work?
Hi,
Apologies for the typo.
Infact, Waitclks must be scaled as below:
AD5940_Delay10us(WaitClks/100);
instead of
AD5940_Delay10us(WaitClks);
1) Since in the above code, wakeup timer is not used, measurement is not periodically triggered, Measure() need to be called for each measurement, hence called inside AppBIAISR().
2) ADC must be turned on only for sampling the input. It should not be kept on always. Otherwise data fifo will be filled with junk data.
In the above code, WG is kept on always.
3) Floating switches after measurement is a good practice but optional. It is not reflected in the waveform captured above because switches are closed for a negligibly small duration.
4) Toggling the GPIO_Pin2 helps check that measurement is happening and also to keep count of measurements, by monitoring GPIO2.
5) Measure() is not using sequence in the above code as measurement is not required to be triggered by timer and sequence can run only at 32kHz clock.
Hence its sequence is already removed in the above code.
Below is the BIA measurement output I got for the above code for a 100 Ohm resistive load:
Hello AD5940-Build Time:11:10:34
Freq:50000.00 RzMag: 99.953804 Ohm , RzPhase: 1.029252
Freq:50000.00 RzMag: 99.953979 Ohm , RzPhase: 1.020536
Freq:50000.00 RzMag: 99.954971 Ohm , RzPhase: 1.018610
Freq:50000.00 RzMag: 99.958328 Ohm , RzPhase: 1.019177
Freq:50000.00 RzMag: 99.960709 Ohm , RzPhase: 1.021670
Freq:50000.00 RzMag: 99.958328 Ohm , RzPhase: 1.019177
Freq:50000.00 RzMag: 99.951485 Ohm , RzPhase: 1.041997
Freq:50000.00 RzMag: 99.960312 Ohm , RzPhase: 1.015318
Freq:50000.00 RzMag: 99.961296 Ohm , RzPhase: 1.013385
Freq:50000.00 RzMag: 99.960312 Ohm , RzPhase: 1.015318
Freq:50000.00 RzMag: 99.958328 Ohm , RzPhase: 1.019177
Freq:50000.00 RzMag: 99.958328 Ohm , RzPhase: 1.019177
Freq:50000.00 RzMag: 99.960709 Ohm , RzPhase: 1.021670
Freq:50000.00 RzMag: 99.952477 Ohm , RzPhase: 1.040064
Freq:50000.00 RzMag: 99.956947 Ohm , RzPhase: 1.014751
Freq:50000.00 RzMag: 99.961296 Ohm , RzPhase: 1.013385
Freq:50000.00 RzMag: 99.957932 Ohm , RzPhase: 1.012818
Freq:50000.00 RzMag: 99.955948 Ohm , RzPhase: 1.016677
Freq:50000.00 RzMag: 99.956947 Ohm , RzPhase: 1.014751
Freq:50000.00 RzMag: 99.956947 Ohm , RzPhase: 1.014751
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.957932 Ohm , RzPhase: 1.012818
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.947716 Ohm , RzPhase: 1.035071
Freq:50000.00 RzMag: 99.957932 Ohm , RzPhase: 1.012818
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.956947 Ohm , RzPhase: 1.014751
Freq:50000.00 RzMag: 99.946732 Ohm , RzPhase: 1.037004
Freq:50000.00 RzMag: 99.958923 Ohm , RzPhase: 1.010885
Freq:50000.00 RzMag: 99.948708 Ohm , RzPhase: 1.033138
Freq:50000.00 RzMag: 99.958923 Ohm , RzPhase: 1.010885
Freq:50000.00 RzMag: 99.958923 Ohm , RzPhase: 1.010885
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.960312 Ohm , RzPhase: 1.015318
Freq:50000.00 RzMag: 99.949104 Ohm , RzPhase: 1.039497
Freq:50000.00 RzMag: 99.956947 Ohm , RzPhase: 1.014751
Freq:50000.00 RzMag: 99.947716 Ohm , RzPhase: 1.035071
Freq:50000.00 RzMag: 99.948708 Ohm , RzPhase: 1.033138
Freq:50000.00 RzMag: 99.959908 Ohm , RzPhase: 1.008959
Freq:50000.00 RzMag: 99.957932 Ohm , RzPhase: 1.012818
Freq:50000.00 RzMag: 99.955948 Ohm , RzPhase: 1.016677
Freq:50000.00 RzMag: 99.993782 Ohm , RzPhase: 1.024464
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.958923 Ohm , RzPhase: 1.010885
Freq:50000.00 RzMag: 99.958923 Ohm , RzPhase: 1.010885
Freq:50000.00 RzMag: 99.946342 Ohm , RzPhase: 1.030645
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Freq:50000.00 RzMag: 99.958923 Ohm , RzPhase: 1.010885
Freq:50000.00 RzMag: 99.956947 Ohm , RzPhase: 1.014751
Freq:50000.00 RzMag: 99.959312 Ohm , RzPhase: 1.017244
Thanks, the code provided does work.
I have removed the floating switch part, so the sine wave is continuous as checked on an oscilloscope.
So, this is what I am trying to do now:
I'm injecting the continuous sine wave generated between CEO and Ain1, and measuring the voltage across part of the body (forearm) between Ain2 and 3. This part works.
I'm trying to measure the heart rate, and as you can see it is sort of working, but not quite yet

I want to understand, does some TIA or input current or anything else is trying to stabilize or auto-calibrate periodically? The impedance values shift i.e. either increases or decreases over time as if trying to stabilize or something. Do you know why it could be happening?
PS: In the figure above, don't look at the values but look at the pattern i.e. the the pattern is slanting downwards to the right from left means impedance values are decreasing over time for a fixed electrode position on the body.
Hi,
If the requirement is to measure heart rate, may I know why you are not using the AD5940_ECG example?
May I know if you are testing using eval board or on your custom board?
If using Eval-AD5940BIOZ board with ECG probes stuck on body, AD5940_ECG example gives below measurement output:

Note: Eval board uses AD8233 (heart rate monitor) along with AD5940.
Hmm, good point, I'll probably look into it, I used AD8421 as my IA, but I will check it out, thanks!
So coming back to the slanting issue mentioned above, could you think of anything why it could be happening?
Also, I do appreciate your help in this matter!
Edit: I think the methodology to measure the HRM via AD8233 vs the way I'm doing is different. I'm amplitude modulating the pulse signal vs the conventional way AD8233 acquires the ECG signal. Quick question, when AD8233 is operational, is AD594x injecting current in the body?
Also, whats the max Bia ODR? I can see it's 20 currently.
BIA ODR can go upto 3kHz. However, in Sensorpal, it is limited to 20.
Hi,
No. AD594x doesn't inject any current.
Hi Akila,
Could you please tell me where should I make changes in the code above to get an ODR of 3k Hz? I changed the BIAODR to 3k, but it didn't work.
Shravan
Hi,
Kindly watch the value of MAXODR for different configurations, so that you may choose the config with maximum MAXODR.
(MAXODR is defined in the default BIA example in Github)
MAXODR
So I checked the code and it says:
AppBIACfg.MaxODR = 1/(((AppBIACfg.MeasSeqCycleCount + 10) / 16.0)* 1E-6) ;
I guess this is what you mean?
The other comment is "DFT number and sample frequency decides the maxim ODR", I changed the DFT number to DFTNUM_16384 and it didn't do anything. Also, my DAC freq is below 80kHz.
MAXODR
So I checked the code and it says:
AppBIACfg.MaxODR = 1/(((AppBIACfg.MeasSeqCycleCount + 10) / 16.0)* 1E-6) ;
I guess this is what you mean?
The other comment is "DFT number and sample frequency decides the maxim ODR", I changed the DFT number to DFTNUM_16384 and it didn't do anything. Also, my DAC freq is below 80kHz.
Hi,
Yes. AppBIACfg.MaxODR = 1/(((AppBIACfg.MeasSeqCycleCount + 10) / 16.0)* 1E-6) ;