Post Go back to editing

How many poles are required on magnet ring in off shaft configuration?

Category: Hardware
Product Number: ADA4570

Hello, 
I want to use the ADA4570 to record a steering angle in an off shaft configuration. The maximum steering angle is about 12-15°, so the absolute range is about 30°. I have read the data sheets but can´t find any information wheater the amount of poles on the required magnet ring is relevant. In the data sheet is one picture with 4 pole pairs and anonther with 10. But I have no idea if thats okay with my setup with slow rates and a small range.  Which amount of pole pairs enables the best accuracy?

Thanks for your help! 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.