Hello.
I have a question regarding the filter settings of the evaluation board software.
The setting is selected from the ODR and HPS pull-down menus, but there is
a difference between the values in Table 44 of the data sheet and the setting of 0x28.
I have attached a comparison table, but with the settings of this software, f
or example, ODR250Hz and HPF1.5545E-4xODR, you will not be able to
get a proper output.
I can't tell if the cause is the software or if I'm using it incorrectly.
Bset Regards.
| ADXL355 Filter Register | ||||||||||||
| Possible correct register settings read from the datasheet(HEX) | ||||||||||||
| ODR | ||||||||||||
| 4000 Hz | 2000 Hz | 1000 Hz | 500 Hz | 250 Hz | 125 Hz | 62.5 Hz | 31.25 Hz | 15.625 Hz | 7.813 Hz | 3.906 Hz | ||
| HPF corner frequency | no high-pass filter | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | A |
| 24.7E−4×ODR | 10 | 11 | 12 | 13 | 14 | 15 | 16 | 17 | 18 | 19 | 1A | |
| 6.2084E−4×ODR | 20 | 21 | 22 | 23 | 24 | 25 | 26 | 27 | 28 | 29 | 2A | |
| 1.5545E−4×ODR | 30 | 31 | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 | 3A | |
| 0.3862E−4×ODR | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 | 48 | 49 | 4A | |
| 0.0954E−4×ODR | 50 | 51 | 52 | 53 | 54 | 55 | 56 | 57 | 58 | 59 | 5A | |
| 0.0238E−4×ODR | 60 | 61 | 62 | 63 | 64 | 65 | 66 | 67 | 68 | 69 | 6A | |
| Register values when set by software of EVAL-ADXL355-SDP(HEX) | ||||||||||||
| ODR | ||||||||||||
| 4000 Hz | 2000 Hz | 1000 Hz | 500 Hz | 250 Hz | 125 Hz | 62.5 Hz | 31.25 Hz | 15.625 Hz | 7.813 Hz | 3.906 Hz | ||
| HPF corner frequency | no high-pass filter | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | A |
| 24.7E−4×ODR | A | B | A | B | E | F | E | F | A | B | A | |
| 6.2084E−4×ODR | 14 | 15 | 16 | 17 | 14 | 15 | 16 | 17 | 1C | 1D | 1E | |
| 1.5545E−4×ODR | 1E | 1F | 1E | 1F | 1E | 1F | 1E | 1F | 1E | 1F | 1E | |
| 0.3862E−4×ODR | 28 | 29 | 2A | 2B | 2C | 2D | 2E | 2F | 28 | 29 | 2A | |
| 0.0954E−4×ODR | 32 | 33 | 32 | 33 | 36 | 37 | 36 | 37 | 3A | 3B | 3A | |
| 0.0238E−4×ODR | 3C | 3D | 3E | 3F | 3C | 3D | 3E | 3F | 3C | 3D | 3E | |