I want to monitor the internal temperature of LTM4657 using the LTC2991.
Is TSENSE+ TSENSE- pins compatible with the LTC2991 remote diode temperature sensing ?
Thanks
LTC2991
Recommended for New Designs
The LTC2991 is used to monitor system temperatures, voltages and currents. Through the I2C serial interface, the eight monitors can individually measure...
Datasheet
LTC2991 on Analog.com
I want to monitor the internal temperature of LTM4657 using the LTC2991.
Is TSENSE+ TSENSE- pins compatible with the LTC2991 remote diode temperature sensing ?
Thanks
Hi sw123 ,
Yes the LTC2991 is compatible with the Tsense+ and Tsense- of the LTM2657, and you can use it to monitor the temperature of the said device.
If you need any more help regarding this, please feel free to create another question. Thank you.
Regards,
Karlo
I have the following connections:
LTM2657.Tsense+ to LTC2991.V7
LTM2657 Tsense- to LTC2991.V8
When reading the external diode temperature on V7-V8, the temp readings go down as the device heats up.
Did I connect the diode reversed ?
I have the following connections:
LTM2657.Tsense+ to LTC2991.V7
LTM2657 Tsense- to LTC2991.V8
When reading the external diode temperature on V7-V8, the temp readings go down as the device heats up.
Did I connect the diode reversed ?