What is the power consumption when using the one-shot mode?

In a one-shot mode, the ADT7422 has an on and off scenario where the part goes into shutdown after a conversion is complete compared to a normal mode where the part is continuously converting. The current consumption during shutdown is reduced to 2uA when VDD is 3.3V. One shot mode is good for power saving and useful when temperature update speed is not critical.