Post Go back to editing

LTC2984 - control of ADC1, ADC2 and ADC3 configuration...

Can I setup the LTC2984 to simultaneously measure two devices in 4-wire mode with a shared sense resistor?  I would like to connect the sense resistor to ADC1, device 1 connected to ADC2 and device 2 connected to ADC3.is there a way that I can configure this for simultaneous measurement rather than the standard cascade measurement?

Or, is there a way to configure both ADC2 and ADC3 to connect to and measure the same device (redundant measurements)?

In what specific setup cases is the ADC3 used?

Jonathan

Top Replies

    •  Analog Employees 
    Jul 4, 2022 in reply to JCheney +1 verified

    Hi  ,

    Unfortunately, there is no way to configure the three channels of the ADC so that you can use them all simultaneously in your desired application. The ADCs are configured depending on the type…