Post Go back to editing

AD590 temperature sensor

Hi Team,
A few days back, I posted a thread, but till now I don't get any response so I'm posting my thread here again
I am trying to make a temperature sensor using AD590 from a +5V supply.
The V+ pin of AD590 will be connected to the +5V and the V- pin is connected to a 1K resistor and the voltage across the 1K (single-ended) is taken to a buffer using op-amp ADA4805-2.
The op-amp is operated at a +3.3V. I hope the circuit will work fine.
Also, can I use the same circuit set up to measure the temperature if I simply replace the AD590 with a diode like 1N4148?.
The unused op-amp is used as a voltage monitor like in the below circuit. Will it arise any problem with the design?.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.