TMP01FPZ - temperature ?

Hello.

Does the TMP01FPZ chip have an industrial or a regular version?
Why is the operating temperature range of -40 to 85V indicated, if the measurement in the datasheet is 55 ° C to + 125 ° C?

  • 0
    •  Analog Employees 
    on Nov 20, 2020 4:23 AM 15 days ago

    Hi, 

    Apologies for the delayed response. The part is fully specified from -40C to 85C but it can operate from -55C to 125C. As we can see on the spec table there is only typical values for output vptat accuracy and output vref spec for both E and F grades at -55C to 125C as compared with the full min/max of both grades at -40C to 85C.

    Regards,

    Karen